Power Blog Homepage

Building an LED Matrix with Arduino, Powered by CUI Supplies

September 8, 2020 by Ron Stull - 12 Minute Read

Building an LED Matrix with Arduino, Powered by CUI Supplies

Background

With COVID-19 keeping many of us at home, I've been using some of my extra time at home to go through my stockpile of power supplies and electronic components to see what I can do with them. My first project was to make use of some old programmable LED strips left over from the holidays. The result was a 24 x 18 matrix of RGB LED lights (432 RGB LEDs total). The matrix has a total of 144 controllable sections (24 x 6) programmed with a variety of selectable routines.

CUI on LED board
Figure 1: "CUI" on LED board

Board Overview

The board is made of a piece of plywood with 3 5-meter-long strips of LEDs cut up into a total of 24 smaller strips, each containing 18 LEDs. The color of the LEDs is controlled by an Arduino Uno in groups of three (6 groups per strip of 18 LEDs), based on user input from a potentiometer and three buttons. The board is powered by CUI's SDI65-12-U-P6, a 60 W, 12 V, 5 A, ac-dc power supply and two internal +/-5 V rails are supplied by CUI's V7805-1000s. A demultiplexer circuit is used to route data to the LED strips. The Arduino monitors the LED current and controls power to the LEDs through a relay.

LED board block diagram
Figure 2: LED board block diagram
picture of LED board Front
Figure 3: LED board Front
picture of LED board back
Figure 4: LED board back
Category Description QTY
Controller ARDUINO UNO ATMEGA328 EVAL BRD 1
LED Strips 5m 150Leds WS2811 led strip programmable dream color light IP67 Tube waterproof white PCB 3
Power Supply AC/DC DESKTOP ADAPTER 12V 60W 1
MUX Board Demuliplexers and 5V regulator 1
Current Sense Board Current sense and amplifier, with -5V regulator, 5V 1
Relay Board Relay board, 12V 1
Button Board User interface board, three buttons, one potentiometer, 5V 1
Figure 5: Top level BOM

External Power

An SDI65-12-U-P6 external power supply is used as the main power source to the board. It can provide 12 V continuously, up to 5 A. Somewhere between 5 A and 7.5 A the power supply will go into over-current protection and hiccup until the load current falls back down. When this happens, the Arduino will lose power and reset unless its power rail can be held up long enough for the fault to be sensed and corrected. To sense the current and to prevent an OCP from resetting the controller, the LED strips are connected to the 12 V power supply through a current sensing circuit and a relay that is controlled by the Arduino.

Each LED has a maximum current of 18.5 mA. With 432 LEDs that puts the max current at 8 A, which means that under certain conditions it could trigger OCP. But that condition only applies when all red, green, and blue LEDs are on at the same time. A solid red or green at full brightness only requires 2.7 A. After testing I found that 4.5 A would be more than enough for everything I planned to do. The Arduino will monitor the sensed LED current and turn off the relay if the current exceeds ~4.6 A. This leaves 5 W for other circuits.

screengrab of oscilloscope
Figure 6: Test measurement of OCP - Relay (green) goes low when current (purple), sensed by amplifier (light blue), exceeds 4.78 A causing LED voltage (dark blue) to turn off. Max power out was 57.2 W during test

Arduino Uno

The Arduino Uno board, which is based around the Atmel ATmega328, is used to control the system. Communication with the LED strips (or the WS2811 that internally control them) is a single wire pulse-width based communication and is handled by the Adafruit NeoPixel library, which is included in the Arduino IDE. All of the communication, display routines, user interface, and relay control are programmed into and controlled by the Arduino board.

image of arduino uno board with labels
Figure 7: Arduino Uno board
chart showing LED communication timing
Figure 8: WS2811 communication timing

MUX Board

Each of the small strips have a single wire communication line that have been demultiplexed into a single communication line by the mux board, which is controlled by the Arduino Uno. The mux board also serves as the central power distribution point. External power, from the SDI65-12-U, plugs into the mux board directly. The 12 V from the power supply is distributed from the mux board to the relay board and the input of a V7805-1000 switching regulator which converts it to 5V for the demultiplexers. The 5V rail is also output to the Arduino and, through that board, to the button and current sense boards.

photo of MUX board
Figure 9: MUX board
MUX Board Schematic
Figure 10: MUX board schematic
Category Description Ref. QTY
Connector 2.0 x 6.5 mm, 5.0 A, Horizontal, Surface Mount (SMT), Dc Power Jack Connector J8 1
Connector CONN HEADER VERT 10POS 2.54MM J1, J2, J3 3
Slide Switch 5A/120V single pole double throw slide switch S1 1
Wire to board Terminal TERM BLK 2P SIDE ENT 2.54MM PCB J4, J5, J6, J7, J9 5
Wire to board Terminal TERM BLK 2P SIDE ENT 5.08MM PCB J10 1
Switching Regulator DC-DC NON-ISOLATED, 2 A, 8~36 VD DC1 1
Ceramic Capacitor CAP CER 0.1UF 50V X7R RADIAL C3, C4, C5 3
Electrolytic Capacitor CAP ALUM 1UF 20% 50V RADIAL C2 1
Al Polymer Capacitor CAP ALUM POLY 470UF 20% 16V T/H C1 1
LED LED GREEN DIFFUSED T-1 3/4 T/H D1 1
MUX IC 3-8 LINE DECODER/DEMUX 16-DIP MUX0, MUX1, MUX2 3
Resistor RES 1.2K OHM 1/8W 5% CF AXIAL R1 1
Figure 11: MUX board BOM

Current Sense Board

The Current Sense board is part of the over current protection (OCP) circuit. The current to the LEDs flows through a power resistor on this board and the voltage of this resistor, which is proportional to the LED current, is sensed and amplified by an op-amp and output to the Arduino. The amplifier gain is controlled by a potentiometer with a minimum gain of 1 and maximum gain of 11. It is normally set to 5, so that the output is 2.5 A/V of the input signal (2 V at 5 A). A comparator, whose threshold is set by a second potentiometer, detects if the OCP threshold has been crossed, which turns on an LED indicator and outputs a logic signal to the Arduino. This board is powered by the V7805-1000 5V rail coming from the MUX Board. It also internally creates the -5 V rail for the op-amp using a V7805-1000 in its inverting configuration.

photo of current board
Figure 12: Current Sense circuit
schematic of current board
Figure 13: Current Sense board schematic
Category Description Ref. QTY
Resistor RES 5.1K OHM 1/8W 5% AXIAL R2, R8 2
OP-AMP IC OPAMP GP 1 CIRCUIT 8DIP U2, U3 2
Resistor RES 10K OHM 1/8W 5% AXIAL R5, R6, R10 3
LED LED GREEN DIFFUSED T-1 3/4 T/H D1 1
LED LED RED DIFFUSED T-1 3/4 T/H D2 1
Transistor MOSFET N-CH 60V 200MA TO-92 Q1, Q2 2
Wire to board Terminal TERM BLK 2P SIDE ENT 2.54MM PCB J1, J2 2
Ceramic Capacitor CAP CER 0.1UF 50V X7R RADIAL C2, C3, C4 3
Switching Regulator DC-DC NON-ISOLATED, 2 A, 8~36 VD U1 1
Resistor RES 470 OHM 1/8W 5% AXIAL R1 1
Capacior CAP ALUM 47UF 20% 25V THRU HOLE C1 1
Resistor RES CHAS MNT 0.1 OHM 5% 16W R4 1
Ceramic Capacitor CAP CER 0.01UF 50V X7R RADIAL C5 1
Trim Pot TRIMMER 10K OHM 0.2W PC PIN TOP R3 1
Trim Pot TRIMMER 50K OHM 0.2W PC PIN TOP R7 1
Figure 14: Current Sense board BOM

Relay Board

The relay board is a simple relay and driver. When the control input goes high the relay turns power on to the LEDs and when it goes low power is removed from the LEDs. This board runs on 12 V coming from the SDI65-12-U-P6 via the MUX Board.

photo of relay board
Figure 12: Relay board
relay board schematic
Figure 13: Relay board schematic
Category Description Ref. QTY
Wire to board Terminal TERM BLK 2P SIDE ENT 2.54MM PCB J1, J2, J3 3
Transistor Bipolar (BJT) Transistor PNP 40V 200MHz 600mW Through Hole TO-92 Q1 1
Transistor N-Channel 60V 200mA (Ta) 400mW (Ta) Through Hole TO-92-3 Q2 1
Resistor RES 2.2K OHM 1/8W 5% AXIAL R1 1
Resistor RES 110K OHM 1/8W 5% CF AXIAL R3 1
Resistor RES 1.2K OHM 1/8W 5% CF AXIAL R2 1
Relay RELAY GEN PURPOSE DPDT 5A 24V K1 1
Figure 14: Relay board BOM

Button Board

The user can control the brightness of the LEDs via a potentiometer. Three buttons allow the user to cycle through a variety of display routines and color settings. This board is powered by 5 V coming from the V7805-1000 on the MUX Board.

[IMGALT]
Figure 14: Button board
[IMGALT]
Figure 15: Button board schematic
Category Description Ref. QTY
Buttons SWITCH PUSHBUTTON SPST 1A 30V S1, S2, S3 3
Wire to board Terminal TERM BLK 2P SIDE ENT 2.54MM PCB J1, J2, J3 3
Ceramic Capacitor CAP CER 0.1UF 50V X7R RADIAL C2 1
LED LED GREEN DIFFUSED T-1 3/4 T/H D1 1
Resistor RES 4.7K OHM 1/8W 5% AXIAL R1 1
Electrolytic Capacitor CAP ALUM 10UF 20% 16V RADIAL C1 1
Resistor RES 110K OHM 1/8W 5% CF AXIAL R2, R3, R4 3
Potentiometer POT 10K OHM 1/5W PLASTIC LINEAR R5 1
Figure 16: Button board BOM

Results

After the boards were soldered and assembled it was time to program some display routines. With the buttons the user can cycle through different routines, turn all of the LEDs on and off, and cycle solid colors, and a potentiometer allows the brightness of the LEDs to be adjusted. However, with limited memory, there's a limit to the number and complexity of the routines.

For the first routine (before I finished adding all of the LED strips) I replaced the potentiometer with an external analog input. A microphone and a level detection circuit were applied to this input and the mic volume controlled the LEDs.

Please accept cookies to play this YouTube video.
Learn more about cookies.

Another routine was a bouncing square whose color would change when it hit an edge.

Please accept cookies to play this YouTube video.
Learn more about cookies.

Finally, I added an all-white setting to test the OCP function. When the brightness is turned up it will trigger the OCP circuit. The following clip also demonstrates the button board toggling the programmed display routines.

Please accept cookies to play this YouTube video.
Learn more about cookies.

You May Also Like


Have comments regarding this post or topics that you would like to see us cover in the future?
Send us an email at powerblog@cui.com

Ron Stull

Ron Stull

Power Systems Engineer

Ron Stull has gathered a range of knowledge and experience in the areas of analog and digital power as well as ac-dc and dc-dc power conversion since joining CUI in 2009. He has played a key role on CUI’s Engineering team with responsibilities including application support, test and validation, and design. Outside of power engineering Ron can be found playing guitar, running, and touring the outdoors with his wife, where their goal is to visit all of the U.S. National Parks.

Need More Info?

Like this blog post?

Sign up to get the latest articles straight into your inbox.


Privacy Policy

This site is protected by reCAPTCHA and the Google Privacy Policy and Terms of Service apply.

*注意:新闻通讯当前仅提供英文版。
 
Powered by Translations.com GlobalLink OneLink SoftwarePowered By OneLink