CUI Expands Its Line of AC-DC Power Supplies for Industrial, IoT, and EV Applications

12/12/2023


CUI Expands Its Line of AC-DC Power Supplies for Industrial, IoT, and EV Applications

Tualatin, OR. [Dec 12, 2023] CUI Inc, a Bel group company, announced the addition of three, chassis mount ac-dc power supplies housed in compact metal cases with the VGS-500, VGS-350D, and VGS-200E series line of products.

The ultra-slim designs make the power supplies appropriate for industrial and IoT use in harsh environments for inductive load applications such as motors, relays, and contactors. The power supplies are also well suited for the growing deployment of electric vehicle charges.

With universal input voltage 85-305 VAC or 120-430 VDC and a wide operating temperature (-40 C to +85 C), the new products from CUI Inc, exceed competitors in the space both in voltage and temperature range. The VGS-200E also has a better MTBF rating over competing products, up to 300,000 hours. All products feature bottom and side installation and are certified to the EN 62368 safety standard with an operating altitude of up to 5,000m.

The new VGS power supply series are available immediately. Please contact CUI Inc for OEM pricing or modified and custom designs.

  • Summary
  • Product series: VGS-500, VGS-350D, VGS-200E
  • Applications:  Industrial, IoT
  • Distribution availability:  Digikey, Mouser, and Farnell Electronics

About Bel

CUI Inc is a Bel group company (NASDAQ: BELFA and BELFB). Bel designs, manufactures and markets a broad array of products that include circuit protection, connectors, cable assemblies, discrete components, magnetics and power supplies. The company serves a global market and operates facilities around the world.

Media Contact:

Theresa Schroeder
Theresa.Schroeder@belf.com


Press Images

Web | Print
 
Powered by Translations.com GlobalLink OneLink SoftwarePowered By OneLink