Power Forward:Staggering Rise in Internet Traffic – Forecast to Pass One Zettabyte in 2016

2014年8月22日


Power Forward:Staggering Rise in Internet Traffic – Forecast to Pass One Zettabyte in 2016

In the August 2014 EDN Power Forward blog post, Mark Adams, Senior Vice President at CUI, discusses the staggering rise in Internet traffic and how CUI is making it their mission to meet these challenges head on.

The article begins, "We don’t necessarily stop to think about it, but if we did, we’d probably realize that our use of the Internet, and particularly the amount of data we consume, has dramatically increased, even in just the past year.Not surprisingly, key factors in this rise are the demand for video streaming, the number of mobile devices now connected to the Internet, and the ever-wider adoption of cloud computing."

"Computer processors, not least those from Intel, continually strive to reduce power with every successive generation, as do many of the other electronic components used in servers and networking devices.However these improvements alone are unfortunately not enough to offset the increased performance requirements needed to keep pace with the skyrocketing demands of this market."

However, CUI's wide range of high efficiency power supplies are, "...designed specifically to deliver the performance needed as data usage pushes towards the zettabyte."

Read the full article on EDN.com

Learn more about CUI's power product offering





 
Powered By OneLink