CUI's NDM3Z-90 Series Selected as a Finalist for the Golden Mousetrap Awards

2016年2月23日


CUI's NDM3Z-90 Series Selected as a Finalist for the Golden Mousetrap Awards

CUI's NDM3Z-90 series was named as a finalist for the 2016 Golden Mousetrap Awards by Design News.The 90 A Novum® digital POL dc-dc converter module series was recognized in the Electronics and Test:“模拟/功率管理/控制”类奖项。The Golden Mousetrap Awards celebrates the success of the people, companies and technologies that are driving progress in today’s U.S. design and manufacturing industries.

The NDM3Z-90 family is the latest generation of digital POL modules from CUI's Novum® product family.Designed specifically to address the increasing current needs of the latest processors, FPGAs and other advanced integrated circuits, the NDM3Z-90 sets new benchmarks in current density and efficiency.Rated to output 90 A, this family packs more power into a non-isolated module than anything else on the market.

Additional information about the 2016 Golden Mousetrap Awards can be found here.

Learn more about Novum’s NDM3Z-90 series





 
Powered By OneLink